Part Number: TMS320F28388D
Hi Team,
I am using TMS320F28388 controller with CCS 11.
While writing the program I have to use a structure like below.
struct HostReply
{
uint16_t Length;
uint32_t BoardStatus;
uint32_t SignalStatus;
union
{
uint16_t Data; // for Read, CRC16 for Write
uint16_t CRC16; // so that sizeof(HostReply) = sizeof(Length) + sizeof(BoardStatus) + sizeof(CRC16)
} Data_CRC;
};
But when I copy the structure data to a buffer, the Length variable is added with extra 2bytes of data. I understood this is structure padding and tried to avoid that using #pragma packet(1) header.
But got a warning like #163-D unrecognized #pragma.
Can you help me to fix this issue and pack the structure properly.
Thanks in advance
Dipin