Part Number: TMS320F28069M
Greetings! I am experiencing some difficulties with FLASH programming TMS320F28069M. So I finally took the example Example_2806xFlash and I tried to FLASH program my uC -> no effect. My board is base on LAUNCHXL-F28069M. So I have 3 switch keys -> on TRST, SDO and GPIO34. So i`ve tried multiple combinations of these switches -> the program is running with the probe connected, but when I disconnect it, nothing happens. Is there a specific procedure for this exact controller? For example putting the controller in waiting state, next swtching to emulation boot for example? The linker file is by default F28069.cmd. The only change I`ve made to the program is that i switch GPIO pin with mine...
Thanks!
PP: My probe is XDS100v3!