Other Parts Discussed in Thread: SYSCONFIG
Hello,
I have a problem with passing/injecting signals from CLB1 to EQEP1. I used XBAR and CLB XBAR to route QEPA and QEPB signals to CLB and then just pass them from input to output.
Problem is, that if I connect the signals to OUTLUT_0 and OUTLUT_1 and then enable outputs 8 and 9, the EQEP1 shows nonsense values. If I pass them from CLB to PWMA/B they look as they should.
I tried to route the QEPA/B signals to other outputs, but with no luck. The question is: where are QA and QB or are they even connected to EQEP1 module ?