This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to program LAUNCHXL-F280049C + BOOSTXL-BUCKCONV to just simply demo the vout at scope for now.
The TI sale website says the boostxl-buckconv is very compatible with Launchxl-f280049c, but, I have not found any existing TI built-in CCS project can run this buck converter test module.
1. So far, I cannot find any related CCS program in C2000WARE-SDK_4_02_00_00 can run the boosterxl-buckconv module.(let me know if i'm wrong)
2. And so far, after I downloaded the C2000WARE_DIGITALPOWER_SDK_4_02_00_00, for some reasons, I cannot import the PowerSuite's TIDM_DC_DC_BUCK's F28004x. (looks like the CCS cannot detect it)
3. I tried to download the ControlSuite's PowerSuite. but, they dont have F28004x, they only have F28069 version.
What is my shot here? I just want to have a CCS code to run the BOOSTXL EVA module.
Please advises! thanks!
Hi,
Due to holiday break, lot of engineers are out of office. Please expect response by next week.
Please take a look at the solution at:
C:/ti/c2000/C2000Ware_DigitalPower_SDK_4_02_00_00/solutions/tidm_dc_dc_buck
Regards, Santosh
Hi,
It is available in DPSDK 4.02, shown below.
It is supported with LAUNCHXL-F280049C.
I am also able to import the 49C based code by clicking the "Import F280049C project " in the screenshot below.
Hello,
I'm able to get the your attached page, but I don't see the project is being added after I click on "import F280049C project", attached the page after i clicked on it.
Then, if I clicked on browse software and examples, it kinda circled back to the first attached pictures.
Still not sure how to do this.
I am not sure what is going on with that, which seems like a software installation issue. Please try install the DPSDK or CCS if necessary.