Hi,
Iam trying to write data into F-RAM(FM25W256, 32K*8 Serial(SPI)F-RAM ) which is 8-bit accessible(TX/RX), from SPI configured in FIFO mode with the support of DMA in controller.
I need to transfer an array of 16-bit parameters each, when only 8-bit is accepted by FRAM, but transfer size(DATASIZE) is limited to a minimum of 16-bit value in DMA.
Please let me know, if there is any way to overcome this issue.
Thanks,
Shreni. P