Other Parts Discussed in Thread: FM22L16, C2000WARE
Hi,
I've been working on my customized board using example code to access EMIF for FM22L16 (18 address lines & 16 data lines) .
The hardware pins are properly mapped. I can perform the reading and writing on the same FM22L16 by using GPIO.
I tried the example code reference C:\ti\c2000\C2000Ware_2_01_00_00\driverlib\f2837xd\examples\cpu1\emif\emif_ex1_16bit_asram code
I'm able to perform the write operation but can't access the reading.
I couldn't access the dedicated address assign for cs2 pin which is 0x0010 0000 I'm unable to perform read operation on this specific address.

Please find the attach file to get more clarification & do let me know if it is possible to configure the EMIF with FM22L16.
Thanks & regards
Sonam