This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: LIN as SCI mode initialized by Sysconfig

Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG

Dear Champs,

I am asking this for our customer. 

Because there are only two SCI modules, the user has to use LIN as SCI for more SCI usage.

1. Can we use Sysconfig to initialize LIN as SCI?

2. If yes, is there any example? If not, when can we have that?

3. There are some registers in LIN module used for baud rate setting, like BRSR register. Are they on Sysconfig?

Wayne Huang

  • Hi Wayne,

    Thanks for your post. Let me answer the questions below:

    1.

    Can we use Sysconfig to initialize LIN as SCI?

    SCI mode is currently not available in Sysconfig for LIN

    2.

    If yes, is there any example? If not, when can we have that?

    See #1 above, unfortunately no support yet for LIN-SCI mode, with no timeline currently known.

    3.

    There are some registers in LIN module used for baud rate setting, like BRSR register. Are they on Sysconfig?

    Baud rate is not available in LIN Sysconfig at this time.

    Regards

    Vince