Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Dear Champs,
I am asking this for our customer.
With C2000ware V5.02, we have LIN in SCI mode linked with DMA in Sysconfig.
Questions:
1. If the user only needs to use LIN in SCI mode for TX DMA request, is interrupt Line 0 required?
See below, the user is very confused.
After this code to enable TX_DMA trigger,

2. Based on the description below, does that mean TX interrupts and TX DMA are mutually exclusive? Only one of them can be used?

3. Why is there a warning below by default?
The user wants to use SCITD of LIN module in SCI mode.
How does the user write SCITD in Sysconfig as TX DMA destination address?