This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280023: Issue with DMA byte transfer from LIN in SCI mode

Part Number: TMS320F280023
Other Parts Discussed in Thread: C2000WARE

I am trying to use a LIN module configured to SCI mode with single buffer along with a DMA module to transfer the received data to memory after each byte is received.  Starting with the C2000WARE example program "lin_ex3_sci_dma", I modified the LIN configuration to disable multi buffer mode and reconfigured the DMAs to transfer a single byte per burst.  While the modified program appears to successfully load and transmit the data via the transmit DMA, the receive DAM will not transfer the data from the Rx buffer.  Through experimentation I was able to make it work by adding an initial force trigger of the receive DMA engine to get it started.  What I can't figure out is why the receive DMA ignores RX DMA Request until after I issue a force trigger?

Modified source file is attached with all changes identified with "//modified".

//#############################################################################
//
// FILE:   lin_ex3_sci_dma.c
//
// TITLE:  LIN SCI MODE Internal Loopback with DMA
//
//! \addtogroup driver_example_list
//! <h1> LIN SCI MODE Internal Loopback with DMA </h1>
//!
//! This example configures the LIN module in SCI mode for internal loopback
//! with the use of the DMA. The LIN module performs as SCI with a set
//! character and frame length in multi-buffer mode. When the transmit buffers
//! in the LINTD0 and LINTD1 registers have enough space, the DMA will transfer
//! data from global variable sData into those transmit registers. Once the
//! received buffers in the LINRD0 and LINRD1 registers contain data,the DMA
//! will transfer the data into the global variable rdata.
//!
//! When all data has been placed into rData, a check of the validity of the
//! data will be performed in one of the DMA channels' ISRs.
//!
//! \b External \b Connections \n
//!  - None
//!
//! \b Watch \b Variables \n
//!  - \b sData - Data to send
//!  - \b rData - Received data
//!
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"

//
// Defines
//
#define BURST       4
#define TRANSFER    32
#define CHAR_LENGTH     8
#define FRAME_LENGTH    8

//
// Configure the Baud Rate to 115.207kHz
//
uint32_t PRESCALER=0x000001a;
uint16_t DIVIDER=0x0002;

//
// Globals
//
uint16_t sData[128];
uint16_t rData[128];


//Place buffers in GSRAM
#pragma DATA_SECTION(sData, "ramgs0");
#pragma DATA_SECTION(rData, "ramgs0");

volatile uint16_t done = 0;         // Flag to set when all data transfered

//
// Function Prototypes
//
void initDMA(void);
void configureSCIMode(void);
__interrupt void dmaCh5ISR(void);
__interrupt void dmaCh6ISR(void);


//
// Main
//
void main(void)
{
    uint16_t i;
    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Initialize GPIO
    //
    Device_initGPIO();

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();
    EINT;
    ERTM;

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    // This registers the interrupt handler in PIE vector table.
    //
    Interrupt_register(INT_DMA_CH5, &dmaCh5ISR);
    Interrupt_register(INT_DMA_CH6, &dmaCh6ISR);

    //
    // Enable the DMA interrupt signals
    //
    Interrupt_enable(INT_DMA_CH5);
    Interrupt_enable(INT_DMA_CH6);

    //
    // Initialize the DMA
    //
    initDMA();

    //
    //Initialize the LIN Module
    //
    LIN_initModule(LINA_BASE);

    //
    // Configure the LIN module to operate in SCI mode
    //
    configureSCIMode();

    //
    // Initialize the data buffers
    //
    for(i = 0; i < 128; i++)
    {
       sData[i]= i;
       rData[i]= 0;
    }

    //
    // Wait for the SCI receiver to be idle
    //
    while(!LIN_isSCIReceiverIdle(LINA_BASE));

    //
    // Wait until space is available in the transmit buffer.
    //
    while(!LIN_isSCISpaceAvailable(LINA_BASE)){}

    //
    //Initiate transfer through a CPU write
    //
    LIN_sendData(LINA_BASE,(unsigned int*)0xFFFF);

    //
    // Start the DMA receive channel
    //
    DMA_startChannel(DMA_CH6_BASE);

    //
    //Start the DMA transmit channel
    //
    DMA_startChannel(DMA_CH5_BASE);


    //////////////////////////////////////////////////////////
    //////////////////////////////////////////////////////////
    //////////////////////////////////////////////////////////
//Modified - Added force trigger of Rx DMA to get it started.  Why is this needed?
    while (!LIN_isRxReady(LINA_BASE));
    DMA_forceTrigger(DMA_CH6_BASE);

    //
    //Wait until the DMA transfer is complete
    //
    while(!done);

    //
    //When the DMA transfer is complete the program will stop here
    //
    ESTOP0;

}

//
// Function to configure LIN in SCI Mode
//
void
configureSCIMode(void)
{
    //
    // Enter LIN reset state to perform configurations
    //
    LIN_enterSoftwareReset(LINA_BASE);

    //
    // Switch LIN into SCI mode
    //
    LIN_enableSCIMode(LINA_BASE);

    //
    // Set the SCI communication mode to idle line
    //
    LIN_setSCICommMode(LINA_BASE, LIN_COMM_SCI_IDLELINE);

    //
    // Set SCI to transmit one stop bit
    //
    LIN_setSCIStopBits(LINA_BASE,LIN_SCI_STOP_ONE);

    //
    // Disable parity check
    //
    LIN_disableSCIParity(LINA_BASE);

    //
    // Enable multi-buffer mode
    //
//Modified
//    LIN_enableMultibufferMode(LINA_BASE);
    LIN_disableMultibufferMode(LINA_BASE);

    //
    // Module set to complete operations when halted by debugger
    //
    LIN_setDebugSuspendMode(LINA_BASE, LIN_DEBUG_COMPLETE);

    //
    // Set character length as 8-bits
    //
    LIN_setSCICharLength(LINA_BASE, CHAR_LENGTH);

    //
    // Set to 1 character in response field
    //
//Modified
//    LIN_setSCIFrameLength(LINA_BASE, FRAME_LENGTH);
  
    //
    // Set the Baud Rate
    //
    LIN_setBaudRatePrescaler(LINA_BASE, PRESCALER, DIVIDER);

    //
    // Enable Internal Loopback mode
    //
    LIN_enableIntLoopback(LINA_BASE);

    //
    //Enable the DMA for transmission
    //
    LIN_enableSCIInterrupt(LINA_BASE, LIN_SCI_INT_TX_DMA);

    //
    //Enable the DMA to receive
    //
    LIN_enableSCIInterrupt(LINA_BASE, LIN_SCI_INT_RX_DMA);


    // Exit LIN reset state
    //
    LIN_exitSoftwareReset(LINA_BASE);
}

//
// DMA setup for both TX and RX channels.
//
void initDMA()
{
    //
    // Initialize DMA
    //
    DMA_initController();

    //
    // Configure DMA Ch5 for TX. When there is enough space in the buffers found in
    // the LINTD0 and LINTD1 registers, data will be transferred from the sdata buffer
    // to the LIN's transmit registers. The destination address is configured to start
    // in the most significant part of the LINTD1 register (TD4/TD5 transmit buffers)and
    // move two address's down with every burst until it fills up the least significant
    // part of the LINTD0 register (TD2/ TD3 transmit buffers).After every transfer of
    // 4 bursts the destination address is brought back to the address of the TD4/TD5
    // buffers contained in the LINTD1 register.
    //
//Modified
//    DMA_configAddresses(DMA_CH5_BASE, (uint16_t *)(LINA_BASE + LIN_O_TD1+2), sData);
    DMA_configAddresses(DMA_CH5_BASE, (uint16_t *)(LINA_BASE + LIN_O_SCITD), sData);
//Modified
//    DMA_configBurst(DMA_CH5_BASE, BURST, 1, -2);
    DMA_configBurst(DMA_CH5_BASE, 1, 0, 0);
//Modified
//    DMA_configTransfer(DMA_CH5_BASE, TRANSFER, 1, 6);
    DMA_configTransfer(DMA_CH5_BASE, 128U, 1, 0);

    DMA_configMode(DMA_CH5_BASE, DMA_TRIGGER_LINATX, DMA_CFG_ONESHOT_DISABLE |
                   DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);

    //
    // Configure DMA Ch5 interrupts
    //
    DMA_setInterruptMode(DMA_CH5_BASE, DMA_INT_AT_END);
    DMA_enableInterrupt(DMA_CH5_BASE);
    DMA_enableTrigger(DMA_CH5_BASE);





    //
    // Configure DMA Ch6 for RX. When the buffers found in the LINRD0 and LINRD1
    // registers are full, data will be transferred to the rdata buffer. The source
    // address is configured to start in the most significant part of the LINRD1
    // register (RD4/RD5 receive buffers) and move two address's down with every
    // burst until it transfers the least significant part of the LINTD0 register
    // (RD2/ RD3 receive buffers).After every transfer of 4 bursts the source
    // address is brought back to the address of the RD4/RD5 buffers contained in
    // the LINRD1 register.
    //
//Modified
//    DMA_configAddresses(DMA_CH6_BASE, rData,(uint16_t *)(LINA_BASE + LIN_O_RD1+2));
    DMA_configAddresses(DMA_CH6_BASE, rData,(uint16_t *)(LINA_BASE + LIN_O_SCIRD));
//Modified
//    DMA_configBurst(DMA_CH6_BASE, BURST, -2, 1);
    DMA_configBurst(DMA_CH6_BASE, 1, 0, 0);
//Modified
//   DMA_configTransfer(DMA_CH6_BASE, TRANSFER, 6, 1);
    DMA_configTransfer(DMA_CH6_BASE, 128U, 0, 1);

    DMA_configMode(DMA_CH6_BASE, DMA_TRIGGER_LINARX, DMA_CFG_ONESHOT_DISABLE |
                   DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);

    //
    // Configure DMA Ch6 interrupts
    //
    DMA_setInterruptMode(DMA_CH6_BASE, DMA_INT_AT_END);
    DMA_enableInterrupt(DMA_CH6_BASE);
    DMA_enableTrigger(DMA_CH6_BASE);
}

//
// DMA Channel 5 ISR
//
__interrupt void dmaCh5ISR(void)
{
    DMA_stopChannel(DMA_CH5_BASE);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
    return;
}

//
// DMA Channel 6 ISR
//
 __interrupt void dmaCh6ISR(void)
{
    uint16_t i;
    DMA_stopChannel(DMA_CH6_BASE);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);

    //
    //Check for data integrity
    //
    for(i=0; i<128; i++)
    {
        if(rData[i] !=i)
        {
           //Something went wrong, rdata doesn't contain expected data.
           ESTOP0;
        }
    }

    done = 1;
    return;
}

  • Don,

    let me route this to our LIN expert!

    Will get back to you today!

    Nima

  • Hi Don,

    It's possible that the data has arrived before the trigger was enabled. Can you see if the data is already in the buffer before the "DMA_startChannel" occurs? I believe that would cause this.

    Regards,

    Vince

  • Hi Vince,

    Thanks for the suggestion.  However, I don't believe that is the issue as the Receive DMA is enabled before any data is sent.  I have also verified that before the first byte is sent that the LIN RXRDY flag is cleared as well as the Receive DMA TRANSFERSTS and PERINTFLG flags indicating that no data has been received by the LIN and no trigger has been received by the Receive DNA.   

  • Hi Don,

    For the LIN-SCI side of things, if you're not in multi-buffer mode, then you need to check these things that are needed :

    1. Are there any receive errors in the LIN/SCI module? Check all error registers, and if any error is set, then DMA request will not occur.

    2. Is there actually data in the buffer when you're expecting it? Particularly in RD7. If there is nothing on the first receive, then the DMA request will not be sent.

    3. Are the SET RX DMA bits set? If not, DMA request will not be sent.

    4. Is the "SET RX DMA ALL" bit set and you are in multiprocessor mode? If in multiprocessor mode, and the DMA ALL bit is set incorrectly, then DMA request will not be sent for either data frames or address frames (depending on how you have it set). This is specific to multiprocessor mode.

    5. Is the SLEEP bit set? If it is set, then the DMA request will not be sent.

    If you have ensured all of the above are set/cleared correctly, then this could potentially be a DMA configuration issue. I will contact the DMA expert at that time to verify this.

    Regards,

    Vince

  • Thanks Vince,

    The issue was with “SET RX DMA ALL”.  I did not have it set as I am not using multiprocessor mode.  It appears however that the first byte received in single byte mode does not trigger the DMA unless this is bit set regardless of if you are using multiprocessor mode or not.  All works as expected after setting the bit.  Please let me know if my understanding is incorrect.

    Thanks,

    Don