This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
A co-worker zipped 2 CCS 11.1.0 based projects and put them in a shared folder.
I opened CCS and opened a new workspace folder.
Then I copied the extracted projects to the new workspace.
I imported one with no problems.
This was a working project. However when I attempted a build without making any modifications I got this error and variantsrepeatedly:
"C:/Work_ZipTest/MPGM/mpgm.h", line 321: error #148: declaration is incompatible with "void __error__(char *, uint32_t)" (declared at line 51 of "C:\ti\c2000\Archive\C2000Ware_4_00_00_00\driverlib\f2838x\driverlib\debug.h")
"../ioExpanderDriver.c", line 35: warning #552-D: variable "returnStatus" was set but never used
1 error detected in the compilation of "../ioExpanderDriver.c".
My co-worker in Far Far Away Land does not get these errors. What could be the cause?
Thanks,
John
Update:
I am using C2000Ware 4.1, checking the project product details it looks like he was using 4.0. Don't know if that matters.
C2000Ware v4.0.0.00
Install location: C:/ti/c2000/Archive/C2000Ware_4_00_00_00
Product-type ID: c2000ware_software_package
Dependencies: <none>
John,
Which example you imported from C2000Ware?
Just to make sure I understand the sequence, I am reiterating
Is my understanding correct?
Hi Santosh and Happy Friday.
I do not know if it was started from an example. But it is a project my coworker in Virginia has worked on for many months.
It was working for him and he saved it to a zip file on a network folder.
A little later I retrieved the zip file and extracted the projects.
I created a new workspace folder while starting CCS 11.1.
I copied the project into the new folder.
Next I imported it.
Then I tried to build it without making any changes.
The errors mentioned above occurred during the first build attempt.
I will try to reproduce it today. and let you know.
Santosh - were you able to reproduce the error? I suspect the issue is related to a mismatch with the C2000Ware version.
Ki,
I was not able to reproduce it.
Here are the sequence I followed:
Regards, Santosh
Thanks guys,
I cannot get the archive directories removed from the discovery path. Should I move the directory out of the c:\ti tree or delete it?
I cannot get the archive directories removed from the discovery path. Should I move the directory out of the c:\ti tree or delete it?
CCS will automatically scan in C:/ti for packages and I believe it will search up to three levels deep (though not sure on this). You can try burying it deeper in C:/ti though perhaps it is best just to move it out completely.
However, I am still confused why CCS keeps changing the package version on you if you have both version installed. It should always default to the original version first if both are available.