Part Number: TMS320F28035
Other Parts Discussed in Thread: SFRA
Hi Team,
Here're some issues from the customer may need your help:
The customer is currently working on the routine for BuckBoostBiDir_F2803x. After the actual programming test, it is found that if the output voltage is set too high at the beginning, there will be no output.
It is speculated that it was caused by excessive compensation that exceeded the upper limit of DUTY at the beginning. So the customer wants to study how the 3p3z compensation coefficient is set in the program.
The customer has several questions about the operation of c2000 Compensation Designer:

1. Is control Freq switching the frequency Fsw? In this example, Fsw is 250kHz, so control Freq is 250kHz, right?
2. What does Plant mean in the three curves? This routine is a feedback circuit. Why need to measure the open loop (OL) curve? How is the compensation curve (Comp) considered a good compensation?
3. There are KDC, fz0, fz1, fz2, fp0, fp1, fp2 and other parameters in 3p3z, how to set these parameters?
--
Thanks & Regards
Yale