I have the code below as part of my project in the CCS:
if (t1 < 0 || t2 < 0)
{
char error[] = "Zero voltage width(s) is/are zero, V1 and nV2 are close";
printf("Error %%s is %s\n",error);
}
If the if the "if" condition is met,
(1) I want the error information to pop up on my computer screen.
(2) I don't want further action than for the the debugging process to be halted (or compilation to stop).
Can someone please help me how I can get this done in CSS.