Other Parts Discussed in Thread: C2000WARE
Number: CS1657036
Contact: Alain Gelinas
First name: Alain
Last name: Gelinas
Short description: Encoder Input problem
Email: gelinala@videotron.ca
Company: RETIRED
Company phone:
Language: English
State: Open
Provide case details or comments:
Hi, I bought a LAUNCHXL-F280049C From you on 08-Mar-2023 Order T03951035
It seems to be working right but… I cant get the encoder to work, maybe something I don’t understand. As directed by CLOUGH42 Electronic Leadscrew
LAUNCHXL-F280049C Configuration
J1 = OFF
J2 = OFF
J3 = OFF
S3a = OFF
S3b = OFF
S4 = ON
Connect the encoder Omron E6B2-CWZ6C to J12 = EQEP1
Installed CCS 9.1.0 - C2000 Real Time MCU
Imported Source Code from CLOUGH42 Electronic Lead Screw 1.0.03
Configure Servo Motor
Encoder OMRON E6B2-CWZ6C
define Encoder resolution to 4096
define ENCODER USE EQEP1
I also tried J13 – define ENCODER USE EQEP2
Is there a way I could monitor if pulses are sent to the processor
I tried testing the encoder Powered it with a good 5.0VDC no ripple = A/B/Z output always HI !!!
Perhaps you might have plans for an Encoder Simulator to see if your circuit works ???
Or maybe you have a better plan ?
A little help from TI would be very appreciated.
Thank You
Alain Gelinas