Part Number: TMS320F28022
Other Parts Discussed in Thread: LAUNCHXL-F280049C, TMDSEMU200-U
Hi Team,
Would you kindly assist with the inquiry below?
A customer developed a custom board with the TMS320F28022PTT after programming a LAUNCHXL-F280049C. They encounter no issue programming the board, but they got a stuck-at-zeros faults when trying to test the connection between the CCS and the board through the LAUNCHXL on board XDS110. They have removed the shunts from J101 on the LAUNCHXL, They use a breakout board with the cable from J102 to the appropriate signals on my board. they placed the F28022 into Wait Mode by pulling GPIO37 high before powering it on. After that they applied power, then removed the pull up on GPIO37, and tried manually pulling XRS low with a jumper. After this they attached the LAUNCHXL via J102, already with power on and connected to CCS. the target configuration set to F28022 on CCS for XDS110, with cJTAG and SWD off. nTRST is registering as ~2.9 V with a 10 kR pulldown, and XRS is high, but the test connection always fails with the scan path stuck-at-zero issues.

here is the link to the pin out reference: https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_jtag_connectors.html
I hope you can help. Let me know if you need more information.
Regards,
Marvin