This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Simulation For SDRAM signal using TMS320F28388DZWT controller. able to Observe Non-Monotocity

Part Number: TMS320F28388D

TI.docx

Please find attached document SI analysis simulation observation>

During the Simulation 3 iteration is carried out.

1. Controller Driver (Ti)  with 2-inch length transmission line with 50 Ohms impedance and receiver SDRAM( ISSI).-Observation ringing, Non-monotocity is Observed.

2. Controller Driver(TI) series termination of 18 Ohms and 2-inch length transmission line with 50 Ohms impedance and receiver SDRAM( ISSI)- 

 Observation Non- monotonicity at ViL threshold.

3.Controller Driver (Ti)  with 2-inch length transmission line with 50 Ohms impedance series with series termination of 48 Ohms near receiver SDRAM( ISSI)- Observation Signal are monotonous at Die Level.

kindly please suggest in the placement of resistor,and how to eliminate Non-monotocity in the Signal.

Thanks and regards,

Haripriya S M