This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The half cycle should calculated in 10msec so that my voltage compassion should could be fast using ADC?
Hello,
The precise ADC timings are published in the device technical reference manual (ADC chapter, ADC timings). Assuming 100 MHz SYSCLK/50MHz ADC clock and minimum ACQPS of 80ns, the maximum throughput of each ADC module is 3.45MSPS (290ns per conversion). Factor in the number of conversions (SOCs) you need to perform each control loop cycle and you should have your answer, although I think this ADC should be more than fast enough for your needs.
Ibukun