This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the difference between the TMS320F28377DPTPEP and TMS320F28377DPTPT processors? Looking at the datasheets, the only difference that I notice is the temperature difference (along with the price). Is there any other differences or advantages for the TMS320F28377DPTPEP? Would the same code execute identically on both?
Thanks,
Kevin
it is a different package only. electrically it is the same.
Just to clarify, do you mean only the internal packaging is different? Because TMS320F28377DPTPEP and TMS320F28377DPTPT are both 176-LQFP packages and the pinouts appear identical. Would the same code execute identically on both or would one be faster than the other?
it's the last portion of the first section of the datasheet
Supports Defense, Aerospace, and Medical Applications:
– Controlled Baseline
– One Assembly/Test Site
– One Fabrication Site
– Available in Extended (–55°C to 125°C) Temperature Range
– Extended Product Life Cycle
– Extended Product-Change Notification
– Product Traceability