Part Number: TMS320F28384S
Other Parts Discussed in Thread: C2000WARE
hello, I am using 28388s to develop network functions,
Using Ethernet_ C28x_ config demo from C2000ware to modify my project,
According to the TRM manual, and ensure that the hardware is working properly.
then configuring Device Pins to rmii function, selected external clock for RMII Mode Clocking,
program the PHY_INTF_SEL field in the EMACSS_CTRLSTS register to rmii function,
at last, compile the project and burn .out file to flash,
I use a network cable to connect the PC and target board, and use ping in the CMD command window to check if the connection is normal,
found that no response.
Please help me to find the question, thank you!