This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: Sysconfig Help

Part Number: TMS320F2800157
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Hello All,

I am currently working with the TMS320F2800157QRHBQ1 processor, and I am facing an issue in the Sysconfig file section.

Initially, the configuration opens with the 80-pin version. However, the processor we are using is a 32-pin variant, so I select the 32-pin version from the "switch" section.

After setting a GPIO as an output, I encounter an error. The error message is as follows: "Description Resource Path Location Type cannot set '$assign' to 'GPIO18': No option named GPIO18 defined, valid options are empty_driverlib_project C/C++ Problem".

I have noticed something peculiar: when I build the project initially with the 80-pin configuration, the files located inside the "sysconfig" folder under the "CPU1_RAM" directory are deleted after configuring them for the 32-pin version. I am in need of assistance regarding this matter.

Thank you for your attention to this issue. I would greatly appreciate any help you can provide.

Best regards

EMRE