Hi Team,
1. This snap shot explains why the device need WAIT boot mode in some situation, my confusion comes from the highlight content:

(spruin7b_TMS320F28002x Real-Time Microcontrollers Technical Reference Manual (Rev. B) P124 3.12.1.2 Emulation Code Security Logic (ECSL))
I cannot understand the 'instruction' that executed. If we don't press the RUN button in CCS debug view, the program will not running. Even if some instructions execute before, do these correspond with the secured zone?
2. In P135 3.12.7.7.1 C Code Example to Disable ECSL for C28x-Zone1, there gives a code example of disable ECSL:

What is the location that these code should be place?
--
Thanks & Regards
Yale