Part Number: TMS320F280025
Other Parts Discussed in Thread: UNIFLASH
Hi Team,
Based on the original thread,
I configured the LINKPOINTER, CSMPSWD and GRABSECT/RAM of B0Z1 by using UNIFLASH 8.3.0.4307:
(I used ZSB2, 0x78040)
(PSWD0 from 0xFFFFFFFF to 0xFFFFFFF8)
(All RAM and SECTOR are allocated to Z1)
After these configurations, I can load image and the device will work properly by using uniflash whatever configure the boot mode to boot to FLASH or WAIT boot mode.
Then I want to re-debug this device by using CCS. I populated the DCSM configurations on CCS-->Debug Configurations...-->Target-->Flash Settings for the project that I want to debug:

(I only populated Zone1 because I think I just using this ZONE.) Then I press the debug button(in wait boot mode), and got this error:


C28xx_CPU1: File Loader: Verification failed: Values at address 0x00A000@Program do not match Please verify target memory and memory map. C28xx_CPU1: GEL: File: C:\Users\x1092776\workspace_v12\led_ex1_blinky\CPU1_RAM\led_ex1_blinky.out: a data verification error occurred, file load failed.
How to resolve it?
--
Thanks & Regards
Yale