Part Number: TMS320F28027
Other Parts Discussed in Thread: CCSTUDIO
Using the XDS100v3 with CCStudio to flash my target but I am getting this error message:
"C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 9.11.0.00128)"
Everything seems to be connected properly. The XDS100v3 is brand new and I am using the USB cable provided with it.
Please advise..
Bruce Miller