This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
I am using TMS320F2812 in one of my legacy project, the legacy software seems to have few issues, I am working on fixing them.
The software was build on Texas Instruments Code Composer Studio 2.21.13.
I am not able to find this compiler version in TI website, could you help me in downloading this version IDE.
Thanks,
Veera
Hello Omer,
The legacy project was developed on Code Composer Studio 2.21.13 and it uses DSP BIOS.
The project is developed for TI DSP TMS320F2812
I am not able to open this project file *.pjt in CCS 12.3.
could you guide me how to open this legacy project in current CCS version.
Thanks,
Veera
could you guide me how to open this legacy project in current CCS version.
Please see:
https://dev.ti.com/tirex/explore/node?node=A__ANA-2UvaDVeIvwRHD7a0Sw__ccs_devtools__FUz-xrs__LATEST
While the above article refers to CCS 3.3, the project management system was mostly the same between CCS 2.x and 3.x so the article should still be relevant.
Note that you are attempting quite a jump from migrating a CCS 2.x project to CCS 12.x. Depending on the complexity of the project, it may be a messy migration.
Thankd
ki
I did import the project using import legacy CCS 3.3 project option and tried to build in CCS 12.3
I got bunch of errors, one error I found common in all source file, cannot open source file "std.h" .
I am not able to resolve it also I didn't any option for DSP/BIOS inclusion while importing the project.
could you help with these issues.
Thanks,
Veera
I got bunch of errors, one error I found common in all source file, cannot open source file "std.h" .
Check your project build properties, specifically the include search paths
I am not able to resolve it also I didn't any option for DSP/BIOS inclusion while importing the project.
Please note that:
a) CCS 12 does not come with DSP/BIOS. It needs to be installed separately.
b) CCS Eclipse (CCSv4 and greater) only supports DSP/BIOS version 5.4x and greater that rely on BIOS tcf based configuration files. If you are using a cdb based BIOS configuration file, you are using an older BIOS version (4.x).
Hi,
Below is the build log generated after legacy project was imported using option import legacy CCSV3.3 project
**** Clean-only build of configuration Release_Flash for project pmc ****
"C:\\ti\\ccs1230\\ccs\\utils\\bin\\gmake" -k -j 12 clean -O
DEL /F "pmc.out"
DEL /F "AppMsg.lst" "AppMsgLoader.lst" "AudioIntf.lst" "CodeStartBranch.lst" "CommOp.lst" "CommOpRx.lst" "CommOpTx.lst" "CrcDef.lst" "DSP28_GlobalVariableDefs.lst" "Gpio.lst" "PieCtrl.lst" "ProtIntf.lst" "ProtMsg.lst" "Protocol.lst" "SafeStr.lst" "Serial.lst" "SysCtrl.lst" "Xintf.lst" "ad.lst" "appl_ver.lst" "audio_dio.lst" "boots28.lst" "coastdown.lst" "commutation.lst" "connect.lst" "crc.lst" "errrtn.lst" "ev.lst" "fault.lst" "flash.lst" "flow.lst" "flowtable.lst" "main.lst" "motorctrl.lst" "pca.lst" "pid.lst" "pioneer_alarms.lst" "queue.lst" "speed.lst" "start.lst" "suction.lst" "sw_ver.lst" "task.lst" "unload.lst" "util.lst" "wash.lst"
DEL /F "AppMsg.obj" "AppMsgLoader.obj" "AudioIntf.obj" "CodeStartBranch.obj" "CommOp.obj" "CommOpRx.obj" "CommOpTx.obj" "CrcDef.obj" "DSP28_GlobalVariableDefs.obj" "Gpio.obj" "PieCtrl.obj" "ProtIntf.obj" "ProtMsg.obj" "Protocol.obj" "SafeStr.obj" "Serial.obj" "SysCtrl.obj" "Xintf.obj" "ad.obj" "appl_ver.obj" "audio_dio.obj" "boots28.obj" "coastdown.obj" "commutation.obj" "connect.obj" "crc.obj" "errrtn.obj" "ev.obj" "fault.obj" "flash.obj" "flow.obj" "flowtable.obj" "main.obj" "motorctrl.obj" "pca.obj" "pid.obj" "pioneer_alarms.obj" "queue.obj" "speed.obj" "start.obj" "suction.obj" "sw_ver.obj" "task.obj" "unload.obj" "util.obj" "wash.obj"
DEL /F "AppMsg.d" "AppMsgLoader.d" "AudioIntf.d" "CommOp.d" "CommOpRx.d" "CommOpTx.d" "CrcDef.d" "DSP28_GlobalVariableDefs.d" "Gpio.d" "PieCtrl.d" "ProtIntf.d" "ProtMsg.d" "Protocol.d" "SafeStr.d" "Serial.d" "SysCtrl.d" "Xintf.d" "ad.d" "appl_ver.d" "audio_dio.d" "coastdown.d" "commutation.d" "connect.d" "crc.d" "errrtn.d" "ev.d" "fault.d" "flash.d" "flow.d" "flowtable.d" "main.d" "motorctrl.d" "pca.d" "pid.d" "pioneer_alarms.d" "queue.d" "speed.d" "start.d" "suction.d" "sw_ver.d" "task.d" "unload.d" "util.d" "wash.d"
DEL /F "AppMsg.asm" "AppMsgLoader.asm" "AudioIntf.asm" "CodeStartBranch.asm" "CommOp.asm" "CommOpRx.asm" "CommOpTx.asm" "CrcDef.asm" "DSP28_GlobalVariableDefs.asm" "Gpio.asm" "PieCtrl.asm" "ProtIntf.asm" "ProtMsg.asm" "Protocol.asm" "SafeStr.asm" "Serial.asm" "SysCtrl.asm" "Xintf.asm" "ad.asm" "appl_ver.asm" "audio_dio.asm" "boots28.asm" "coastdown.asm" "commutation.asm" "connect.asm" "crc.asm" "errrtn.asm" "ev.asm" "fault.asm" "flash.asm" "flow.asm" "flowtable.asm" "main.asm" "motorctrl.asm" "pca.asm" "pid.asm" "pioneer_alarms.asm" "queue.asm" "speed.asm" "start.asm" "suction.asm" "sw_ver.asm" "task.asm" "unload.asm" "util.asm" "wash.asm"
DEL /F "CodeStartBranch.d" "boots28.d"
Could Not Find C:\MCS_HVAD\DSP_BIOS\pmc\Release_Flash\pmc.out
Could Not Find C:\MCS_HVAD\DSP_BIOS\pmc\Release_Flash\AppMsg.asm
Could Not Find C:\MCS_HVAD\DSP_BIOS\pmc\Release_Flash\CodeStartBranch.d
Finished clean
**** Build Finished ****
**** Build of configuration Release_Flash for project pmc ****
"C:\\ti\\ccs1230\\ccs\\utils\\bin\\gmake" -k -j 12 all -O
"C:/MCS_HVAD/DSP_BIOS/pmc/preBuildStep_Release_Flash.bat"
1 file(s) copied.
1 file(s) copied.
Building file: "../AppMsg.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="AppMsg.d_raw" "../AppMsg.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'AppMsg.obj' failed
Could Not Find C:\MCS_HVAD\DSP_BIOS\pmc\pmc.hex
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../AppMsg.c".
Compilation terminated.
gmake[1]: *** [AppMsg.obj] Error 1
Building file: "../AppMsgLoader.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="AppMsgLoader.d_raw" "../AppMsgLoader.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'AppMsgLoader.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../AppMsgLoader.c".
Compilation terminated.
gmake[1]: *** [AppMsgLoader.obj] Error 1
Building file: "../AudioIntf.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="AudioIntf.d_raw" "../AudioIntf.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'AudioIntf.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../AudioIntf.c".
Compilation terminated.
gmake[1]: *** [AudioIntf.obj] Error 1
Building file: "../CommOp.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="CommOp.d_raw" "../CommOp.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'CommOp.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../CommOp.c".
Compilation terminated.
gmake[1]: *** [CommOp.obj] Error 1
Building file: "../CommOpRx.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="CommOpRx.d_raw" "../CommOpRx.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'CommOpRx.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../CommOpRx.c".
Compilation terminated.
gmake[1]: *** [CommOpRx.obj] Error 1
Building file: "../CodeStartBranch.asm"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="CodeStartBranch.d_raw" "../CodeStartBranch.asm"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
Finished building: "../CodeStartBranch.asm"
Building file: "../CommOpTx.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="CommOpTx.d_raw" "../CommOpTx.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'CommOpTx.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../CommOpTx.c".
Compilation terminated.
gmake[1]: *** [CommOpTx.obj] Error 1
Building file: "../CrcDef.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="CrcDef.d_raw" "../CrcDef.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'CrcDef.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../CrcDef.c".
Compilation terminated.
gmake[1]: *** [CrcDef.obj] Error 1
Building file: "../DSP28_GlobalVariableDefs.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="DSP28_GlobalVariableDefs.d_raw" "../DSP28_GlobalVariableDefs.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'DSP28_GlobalVariableDefs.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../DSP28_GlobalVariableDefs.c".
Compilation terminated.
gmake[1]: *** [DSP28_GlobalVariableDefs.obj] Error 1
Building file: "../Gpio.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="Gpio.d_raw" "../Gpio.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'Gpio.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../Gpio.c".
Compilation terminated.
gmake[1]: *** [Gpio.obj] Error 1
Building file: "../PieCtrl.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="PieCtrl.d_raw" "../PieCtrl.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'PieCtrl.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../PieCtrl.c".
Compilation terminated.
gmake[1]: *** [PieCtrl.obj] Error 1
Building file: "../ProtIntf.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="ProtIntf.d_raw" "../ProtIntf.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'ProtIntf.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../ProtIntf.c".
Compilation terminated.
gmake[1]: *** [ProtIntf.obj] Error 1
Building file: "../ProtMsg.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="ProtMsg.d_raw" "../ProtMsg.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'ProtMsg.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../ProtMsg.c".
Compilation terminated.
gmake[1]: *** [ProtMsg.obj] Error 1
Building file: "../Protocol.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="Protocol.d_raw" "../Protocol.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'Protocol.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../Protocol.c".
Compilation terminated.
gmake[1]: *** [Protocol.obj] Error 1
Building file: "../SafeStr.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="SafeStr.d_raw" "../SafeStr.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'SafeStr.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../SafeStr.c".
Compilation terminated.
gmake[1]: *** [SafeStr.obj] Error 1
Building file: "../Serial.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="Serial.d_raw" "../Serial.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'Serial.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../Serial.c".
Compilation terminated.
gmake[1]: *** [Serial.obj] Error 1
Building file: "../SysCtrl.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="SysCtrl.d_raw" "../SysCtrl.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'SysCtrl.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../SysCtrl.c".
Compilation terminated.
gmake[1]: *** [SysCtrl.obj] Error 1
Building file: "../Xintf.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="Xintf.d_raw" "../Xintf.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'Xintf.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../Xintf.c".
Compilation terminated.
gmake[1]: *** [Xintf.obj] Error 1
Building file: "../ad.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="ad.d_raw" "../ad.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'ad.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../ad.c".
Compilation terminated.
gmake[1]: *** [ad.obj] Error 1
Building file: "../appl_ver.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="appl_ver.d_raw" "../appl_ver.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'appl_ver.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../appl_ver.c".
Compilation terminated.
gmake[1]: *** [appl_ver.obj] Error 1
Building file: "../audio_dio.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="audio_dio.d_raw" "../audio_dio.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'audio_dio.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../audio_dio.c".
Compilation terminated.
gmake[1]: *** [audio_dio.obj] Error 1
Building file: "../coastdown.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="coastdown.d_raw" "../coastdown.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'coastdown.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../coastdown.c".
Compilation terminated.
gmake[1]: *** [coastdown.obj] Error 1
Building file: "../boots28.asm"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="boots28.d_raw" "../boots28.asm"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
Finished building: "../boots28.asm"
Building file: "../commutation.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="commutation.d_raw" "../commutation.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'commutation.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../commutation.c".
Compilation terminated.
gmake[1]: *** [commutation.obj] Error 1
Building file: "../connect.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="connect.d_raw" "../connect.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'connect.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../connect.c".
Compilation terminated.
gmake[1]: *** [connect.obj] Error 1
Building file: "../crc.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="crc.d_raw" "../crc.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'crc.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../crc.c".
Compilation terminated.
gmake[1]: *** [crc.obj] Error 1
Building file: "../errrtn.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="errrtn.d_raw" "../errrtn.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'errrtn.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../errrtn.c".
Compilation terminated.
gmake[1]: *** [errrtn.obj] Error 1
Building file: "../ev.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="ev.d_raw" "../ev.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'ev.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../ev.c".
Compilation terminated.
gmake[1]: *** [ev.obj] Error 1
Building file: "../fault.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="fault.d_raw" "../fault.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'fault.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../fault.c".
Compilation terminated.
gmake[1]: *** [fault.obj] Error 1
Building file: "../flash.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="flash.d_raw" "../flash.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'flash.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../flash.c".
Compilation terminated.
gmake[1]: *** [flash.obj] Error 1
Building file: "../flow.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="flow.d_raw" "../flow.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'flow.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../flow.c".
Compilation terminated.
gmake[1]: *** [flow.obj] Error 1
Building file: "../flowtable.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="flowtable.d_raw" "../flowtable.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'flowtable.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../flowtable.c".
Compilation terminated.
gmake[1]: *** [flowtable.obj] Error 1
Building file: "../main.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'main.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../main.c".
Compilation terminated.
gmake[1]: *** [main.obj] Error 1
Building file: "../motorctrl.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="motorctrl.d_raw" "../motorctrl.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'motorctrl.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../motorctrl.c".
Compilation terminated.
gmake[1]: *** [motorctrl.obj] Error 1
Building file: "../pca.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="pca.d_raw" "../pca.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'pca.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../pca.c".
Compilation terminated.
gmake[1]: *** [pca.obj] Error 1
Building file: "../pid.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="pid.d_raw" "../pid.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'pid.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../pid.c".
Compilation terminated.
gmake[1]: *** [pid.obj] Error 1
Building file: "../pioneer_alarms.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="pioneer_alarms.d_raw" "../pioneer_alarms.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'pioneer_alarms.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../pioneer_alarms.c".
Compilation terminated.
gmake[1]: *** [pioneer_alarms.obj] Error 1
Building file: "../queue.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="queue.d_raw" "../queue.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'queue.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../queue.c".
Compilation terminated.
gmake[1]: *** [queue.obj] Error 1
Building file: "../speed.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="speed.d_raw" "../speed.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'speed.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../speed.c".
Compilation terminated.
gmake[1]: *** [speed.obj] Error 1
Building file: "../start.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="start.d_raw" "../start.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'start.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../start.c".
Compilation terminated.
gmake[1]: *** [start.obj] Error 1
Building file: "../suction.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="suction.d_raw" "../suction.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'suction.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../suction.c".
Compilation terminated.
gmake[1]: *** [suction.obj] Error 1
Building file: "../sw_ver.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="sw_ver.d_raw" "../sw_ver.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'sw_ver.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../sw_ver.c".
Compilation terminated.
gmake[1]: *** [sw_ver.obj] Error 1
Building file: "../task.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="task.d_raw" "../task.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'task.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../task.c".
Compilation terminated.
gmake[1]: *** [task.obj] Error 1
Building file: "../unload.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="unload.d_raw" "../unload.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'unload.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../unload.c".
Compilation terminated.
gmake[1]: *** [unload.obj] Error 1
Building file: "../util.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="util.d_raw" "../util.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'util.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../util.c".
Compilation terminated.
gmake[1]: *** [util.obj] Error 1
Building file: "../wash.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="wash.d_raw" "../wash.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'wash.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
1 catastrophic error detected in the compilation of "../wash.c".
Compilation terminated.
gmake[1]: *** [wash.obj] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
makefile:177: recipe for target 'all' failed
**** Build Finished ****
could you help me in resolving the errors related with CCS, I see mostly errors are of gmake.
Thanks,
Veera
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/SP00690_PMC/SE-0000-28-5 Rev 004-a Source/include" --include_path="C:/MCS_HVAD/DSP_BIOS/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/SP00690_PMC/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include" --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --preproc_with_compile --preproc_dependency="wash.d_raw" "../wash.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'wash.obj' failed
Command-line error #1966: cannot open source file "C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include": Invalid argument
This is wrong:
--preinclude="C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include"
The --preinclude option is expecting a header file, not a path. Did you add this option? It should go under --include_path if you meant to add it as an include path option.