Part Number: LAUNCHXL-F2800157
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hello all, I am again unable to use the documentation to run a basic blinky application on a freshly unboxed launchpad. This time it's on the F2800157. Here's what's happened so far:
- I import the project, build and try to flash
- It tells me I needed to update the firmware so accept and it completes
- Now CCS will not recognize the device until I eventually decide to reboot and power cycle a number of times
- I successfully run the debugger with the application but see no blinky LED
- I pause the debugger to see what's running and the sources for the function it's executing (sysctl_delay) are for some reason not available
What am I doing wrong? If this is my experience trying to blink an LED on now the 3rd EVK, I fear for when I'm trying to configure complex peripherals.