This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1007: Inductors and capacitor replacement?

Part Number: TIDM-1007

Team,
Customer is looking at TIDM-1007 as base for a project.
But it seems that some of the passives used in TIDM-1007 are difficult to source.

-Can you please help to suggest some replacement for the below and provide comments to the questions?
L103                                                     7448051507                                                     -  7mH Inductor

K100                                                     875B-1CC-F-S-12VDC                                    - Relay, SPDT, 16A, 12VDC, TH                   

            Do you have some suggestion? If not then we can find some replacement part.

L100, L101, L102                             G164005LF                                                        - Inductor, Thoroid, 0.065 ohm, TH

C100, C101, C102, C103               EKMW451VSN221MP40S                            220uF, 450V, TH                                               Do you have some suggestion? If not then we can find some replacement part.

-Alternatively can you provide the key specifications in order to find a suitable replacement?

Thanks in advance,
A.

  • AnBer,

    For L103, yes, you can use Wurth 7448052303.

    For K100, you can use Omron G5LE-1-E-DC12. 

    For L100, L101, L102, yes, Renco RLTI-1328 is what we are using right now.

    For C100, C101, C102, C103, you can use Rubycon 450MXK220MEFCSN22X40.

    Regards,

    Sheng-Yang Yu