Part Number: TMS320F280039C
Other Parts Discussed in Thread: TMS320F280037C, TCAN332, TCAN332G
We have a few TMS320F280039C launchpad and I wanted to know how to use the MCAN modules via simulink. In the C2000 motor control blockset I only see CAN FD pack and unpack blocks. Previously I used the classic CAN with the eCAN recieve and eCAN transmit blocks, but I don't see the option to change those. When I attempt to run the code I get an error as the expected input data type is not CAN FD (it is just set as CAN message). Is there a way to utilize the CAN FD via Simulink?
My second question is how fast can the CAN FD be for the TMS320F280037C MCU. We got the TMS320F280039C launchpad as it was the closest MCU to the one we were planning on using however its onboard CAN transciever is 1Mbps (same as classic CAN). Can either of these MCU run at a faster speed for the MCAN if they have a faster transciever?