Part Number: TMS320F280039C
Dear Champs,
I am asking this for our customer.
Because the user is going to optimize code size, the user wants to clarify how to read from our CCS memory allocation view and .map file.
From below image.
14674 word is code.
3285 word is ro data.
28505 word is rw data.
Questions:
1. ro data means read-only data. So it should be part of flash image. Is it right?
2. rw data means read-write data, so it should be used in RAM. This is the total RAM size that will be used. Is it right?
3. From .map
Flash size will take up 14674 + 3285 = 17959
RAM size will take up 28505
From memory allocation view:
Flash size total is 712 + 14088 + 2870 = 17670, which is almost same as 17959 above. But why is there a difference 17959-17670?
RAM size total is 296 + 1930 + 2048 + 24568 = 28842, which is almost same as 28505. But why is there a difference 28505 - 28842?