Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi Expert,
My customer face a strange issue that they can run Ethercat well on CPU1 and connected to Twincat with emulator connected, that is they will load the code by CCS and run everything ok.
but when they disconnected the emulator and run the device standalone when power on, there is not able to be connected to Twincat,
we thought there may be caused by RAM initialization, but we get all RAM memory at the beginning of main function of both good case and bad case, find that all RAM value and ESC register are the same between these two case, so RAM initialization may not be the root cause.
For the bad case that power on with connected to emulator, only have the issue that Twincat that can not scan the device, other function are normal and no illegal interrupt nor reset event happen.
Could you suggest how to debug this issue?