Part Number: TMS320F28034
Dear All:
Problem Description: The CCS software version I use is V10.4, and there are two compiler versions: V15.12.3 and V20.2.5. The chip used is: DSP_TMS320F28034PNT. At present, there is no problem in using the compiler V15.12.3 for the same project. Using the compiler V20.2.5 will cause the program to be abnormal during operation.
The specific phenomenon is: through simulation, increase the breakpoint way, I found that when jumping to a certain function, one can successfully jump, the other will fail to jump.
First, I want to know if the problem that causes the program exception is caused by a difference in the compiler. Secondly, I wonder if there is any effective solution to make the program run properly on the new compiler(V20.2.5).Finally, I hope that the relevant technician or expert can work with me to reproduce and solve the problem!