Part Number: TMS320F28386D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Hi
There was a report of this error in feb 2023 TMS320F28386D: about CMD Tool error in sysconfig
It was acknowledged as a bug:

I did already then requested a link to follow the progress of this but newer got a reply to that.
And now i see the bug is still present in the latest C2000Ware 5.0 and sysconfig 1.17.
So I kindly request again to get a jira link (or similar) to track progress on this bug.
I still see the bug in my local IDE, and I also reproduced it in the cloud version (see attached file).
How to reproduce.
- Import the example "empty sysconfig dual cpu"
- Add MEMCFG module to both cpu's
- Add CMD module to cpu1 config
- in CMD module, Create a RAMGS mem combination, of 1 or more RAMGS sectors (Fig 1).
- in CMD->Sextion->C28x Compiler section->ramfunc,
load from a flash sector, and run from a RAMGS sector- If you select a "build-in section" like RAMGS7, there is no error.(Fig 2)
- If you selct the mem combination created above, it will show an error about missing MEMCFG. (Fig 3)

Fig1

Fig 2

Fig 3
Project files, the cloud IDE was not able to download it as one tar, so here is the three projects for this setup in separate files.