Part Number: TMS320F28335
Dear experts,
As mentioned in the technical specifications of F28335 about power sequencing-section 7.9.2. I would like to realize timing sequence using OPAMPs, which enables LDOs, that derive 3.3V and 1.9V. Please find the attachment. I found TPS767D301 power supplies IC which derives 3.3V and 1.9V and RESET is also incorporated in the same IC. However, I find using LDOs gives better voltage quality. Therefore I would like to use LDOs with the combination of OPAMPs. OPAMPS takes care of the power sequencing as shown in the figure. Do you think its a right way to do it?
Regards,
Rajesh BN.