Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8301, MOTORWARE
We are using the 28069 processor and the DRV8301. My firmware is very similar to the lab 10. The motor is connected to a gearbox so that on startup it is always loaded to some level but not full load. It has worked very well but we have one issue that we can't isolate and I need assistance. On intermittent occasions the motor seems to stall. It is not often but on those occasions the motor emits a very loud sound that would be described as grinding sound. It is in the motor not the gearbox. The motor will jerk and attempt to run but it is very slowly if at all. It sounds as though the motor is self destructing. If the system is shut down and power restored the issue will go away and it may work correctly for minutes, hours, or days until it occurs again.
We have checked the power supply for any glitches and found none. The circuit design is a replica of the
DRV8301-69M-KIT.
I assumed at first that the motor was hitting a section of the rotation that was problematic and it simply needed a "bump" to get started. That does not seem to be the issue. Due to the gearbox which is connected to a track system it appears the motor stays at exactly the same rotation point when the problem occurs, power is pulled and power is restored. It starts from that exact location just fine.
We have dozens of these in the field and we have a small percentage that exhibit this behavior.
Can someone give some suggestion as to what we should look at to try to trace this down?
Terry Harrison