Part Number: TMS320F2812
Hello,
so far we have used hex2000 and FileIOshell.exe to create a bin from out file. (postbuilding steps under windows)
Since we are now planning to switch to Linux, we would like to create the bin file using tiobj2bin (since FileIOshell.exe cannot be used under Linux).
It works in principle, but unfortunately the byte order in the generated .bin file is swaped compared to the one generated with fileIOshell.
Are there parameters with which one can instruct tiobj2bin to perform a byteswap?
(or is there a way to create a bin file directly with hex2000 at memorywidth 16?)
BR,
Stefan