Part Number: TMS320F28335
Other Parts Discussed in Thread: AMC3330
Dear Experts,
I am working on design of a customized TMS320F28335 based PCB, in which the voltages and currents of the inverter are to be measured, which are in the order of 250A rms, 220V. Hall sensors are placed on the lines, which are off the board. Since the hall sensors are inherently isolated, would you recommend to have another isolation on the board, say AMC3330, which isolates the signal. My worry is, if the isolation is not provided, the micro-controller ground would extend to the inverter stack physically, where 220V switching takes place. Furthermore, the currents are quite high, around 250A, So, the EMI might effect the micro-controller performance.
Please find the current isolation section of the complete schematic attached. I can share the complete schematic in the chat.
My question is, would you recommend to have a double isolation if the hall sensors are placed away from the micrcontroller PCB, or I am just overthinking about EMI-EMC?
Regards,
Rajesh BN.