Part Number: TMS320F28034
Other Parts Discussed in Thread: UNIFLASH
Hi team,
my customer is having the following problem with the program they use to input data on our device:
TI MCU TMS320F28034 used on the converter control board is currently being developed using Blackhawk BHFlashburn_v4.1 for later MCU flashing, but due to the fact that most of the current computers are being upgraded, the Java version has been upgraded to Java 8, while Blackhawk BHFlashburn_v4.1 is only Java 7 compatible. As a result, the Blackhawk BHFlashburn_v4.1 on the new PC is not available. So, only one old PC can be used in the post-development and debugging process, which greatly affects productivity.
Do you suggest any alternatives to Blackhawk BHFlashburn_v4.1?
Best regards,
Riccardo