Hello
the erad module is configured to fire a NMI when the stack pointer reaches a certain address which is defined in the Ref register shown in the attacehed photo, the problem is that : the behavior of that register is not stable sometimes it got the configured value right and the stack overflow testing using recurssive function passes but sometimes that register is loaded with a garbage value that doesn't even fall between the stack boundaries.
so the question is :what is causing that unstable behavior in that register ?


Mahmoud