Other Parts Discussed in Thread: SFRA, PMP23126
Hi ,
Is there any issue with SFRA phase measurement. I have attached SFRA plant response I obtained for PSFB using Vienna rectifier TIDM 1000 code. I edited the code for PSFB requirement for plotting SFRA. I am sensing output voltage single sample only per ISR and not averaging.
Injection amplitude is 0.01
The dc gain of 40db is correct as per theoretical calculations.
However why phase keeps on decreasing after 1kHz ( I understand that after -180, it is decreasing further and therefore jumping to 179 as tan value is same). It can be seen that phase is decreasing at a faster rate even though magnitude is constant after 200 kHz. A double pole would reduce the phase to -180 degree and will keep the phase same thereafter. But here magnitude is remaining same with no decrease indication transfer function zero, but phase starts decreasing at a faster rate. Is the phase measurement correct in SFRA.
I added a digital low pass filter with cut off frequency 10 kHz in the voltage measurement and I am getting following plot.

The addition of know pole at 10 kHz is slowing down the decrease in phase.
Hence, my doubt about phase measurement.
ISR frequency is 50 kHz.
Plant response is being plotted for perturbation around steady state duty of 0.8.
Will averaging four samples of voltage ADC value in a ISR will improve the result.