Part Number: TMS320F2800137
Good afternoon,
I wanted to clarify the behavior of GPIO28 on F2800137RHBR. I am looking to use this pin for SCI boot as SCIA_RX as this is the default value for unprogrammed devices However, this pin is an AGPIO and has the following footnote in the datasheet which states it is by default unconnected.
(3) The GPIOs on these analog pins support full digital input and output functionality and are referred to as AGPIOs. By default, the AGPIOs are unconnected; that is, the analog and digital functions are both disabled. For configuration details, see the Digital Inputs and Outputs on ADC Pins (AGPIOs) section
Can you clarify what happens during the SCI boot mode execution? Will it read from GPIO28 on an unprogrammed device, or does it need to be programmed first?
Thanks!