Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE, UNIFLASH
Hi all,
I try to implement secure flash boot for a while.
I read "Secure BOOT on C2000 Device" application report, "TMS320C28x Assembly Language Tools" user guide and DCSM section in TRM.
I have a theoretical knowledge of the subject.
Now it is time to hands on examples.
-
I examined the example where is located in C2000Ware_4_03_00_00\driverlib\f2838x\examples\c28x\boot.
I will run this code on controlCARD.
I read "How to Run" section (at the beginning of the "boot_ex1_cpu1_cpu2_cm_secure_flash_cpu1.c" ), and i did what is said.
- Application (boot_ex1_cpu1_cpu2_cm_secure_flash_cpu1) is loaded to CPU1.
- Disconnect CPU1.
- Connect CPU1 (In this step, an error occured: failed to parse the previous frame FP. See sss below. I think I can ignore this error for now.)
- Set emulation boot to secure flash boot. (I managed to change the emulation boot mode before. So I am sure that I did)
- Finally, reset CPU1 and resume
After reset, I clicked Resume button. (Resume button dimmed for short time then being appear again.)
I observed LEDs.
CPU1 - LED1 is off. That means Secure Boot failed.
I was expecting at least the LED1 to turn on. (primary secure boot success.)
In addition to "How to Run" section (at the beginning of the "boot_ex1_cpu1_cpu2_cm_secure_flash_cpu1.c" ),
is there anything to do for make this example work ?
For example writing CMAC Key to the OTP region?
(I think this is not necessary because i used default cmac key 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF)
Thank you for your response,
Best regards
Mehmet