This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Writing in OTP memory to change Boot mode settings in C Follow Up

Part Number: TMS320F280049C

Hi,

I'm trying to accomplish the same as in this post, without any luck:

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1097579/tms320f280049c-writing-in-otp-memory-to-change-boot-mode-settings-in-c

Any steps beyond what's in the post?

Thanks for any advice!

The top of my Main:

//
// Included Files
//
#include <cla_pwm_control_shared.h>
#include "driverlib.h"
#include "device.h"
#include "board.h"
#include "math.h"

#pragma DATA_SECTION(OTP_KEY,"OTP_KEY");
#pragma DATA_SECTION(OTP_BMODE,"OTP_BMODE");
#pragma DATA_SECTION(OTP_Boot, "OTP_Boot");
const uint16_t OTP_KEY = 0x5AFF;
const uint16_t OTP_BMODE = 0xFFFF;
const uint16_t OTP_Boot = 0xFF03;
//
// Function Prototypes
//
void initEPWM(void);
void initCLA(void);
uint16_t dutyCalc(uint16_t step, uint16_t amp, uint16_t phase);
void configBMSPS0(void);


//global
uint16_t epwm1_period = 0;
uint32_t frequency = 0;

//
// Main
//
void main(void)
{

And my Linker File:

MEMORY
{
PAGE 0 :
   /* BEGIN is used for the "boot to SARAM" bootloader mode   */

   BEGIN            : origin = 0x080000, length = 0x000002
   RAMM0            : origin = 0x0000F6, length = 0x00030A

   RAMLS0           : origin = 0x008000, length = 0x000800
   RAMLS3           : origin = 0x009800, length = 0x000800
   RAMLS4           : origin = 0x00A000, length = 0x000800
   RESET            : origin = 0x3FFFC0, length = 0x000002

   OTP_BMODE : origin = 0x07800C, length = 0x000001 /* Add by me */
   OTP_KEY : origin = 0x07800D, length = 0x000001 /* Add by me */
   OTP_Boot : origin = 0x07801C, length = 0x000003 /* Add by me */

/* Flash sectors */
   /* BANK 0 */
   FLASH_BANK0_SEC0  : origin = 0x080002, length = 0x000FFE    /* on-chip Flash */
   FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000    /* on-chip Flash */

   /* BANK 1 */
   FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000    /* on-chip Flash */
   FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0    /* on-chip Flash */

//   FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

PAGE 1 :

   BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
//   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMLS1           : origin = 0x008800, length = 0x000800
   RAMLS2           : origin = 0x009000, length = 0x000800
   RAMLS5           : origin = 0x00A800, length = 0x000800
   RAMLS6           : origin = 0x00B000, length = 0x000800
   RAMLS7           : origin = 0x00B800, length = 0x000800

   RAMGS0           : origin = 0x00C000, length = 0x002000
   RAMGS1           : origin = 0x00E000, length = 0x002000
   RAMGS2           : origin = 0x010000, length = 0x002000
   RAMGS3           : origin = 0x012000, length = 0x001FF8
//   RAMGS3_RSVD      : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080
}


SECTIONS
{
   .cinit           : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)
   .text            : >>FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3,   PAGE = 0, ALIGN(4)
   codestart        : > BEGIN       PAGE = 0, ALIGN(4)

   .stack           : > RAMM1        PAGE = 1
   .switch          : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)

#if defined(__TI_EABI__)
   .init_array      : > FLASH_BANK0_SEC1,       PAGE = 0,       ALIGN(4)
   .bss             : > RAMLS5,       PAGE = 1
   .bss:output      : > RAMLS5,       PAGE = 1
   .bss:cio         : > RAMLS5,       PAGE = 1
   .data            : > RAMLS6,       PAGE = 1
   .sysmem          : > RAMLS6,       PAGE = 1
   .const           : > FLASH_BANK0_SEC4,       PAGE = 0,       ALIGN(4)
#else
   .pinit           : > FLASH_BANK0_SEC1,       PAGE = 0,       ALIGN(4)
   .ebss            : >>RAMLS5 | RAMLS6,       PAGE = 1
   .esysmem         : > RAMLS6,       PAGE = 1
   .cio             : > RAMLS5,       PAGE = 1
   .econst          : > FLASH_BANK0_SEC4,    PAGE = 0, ALIGN(4)
#endif

   ramgs0           : > RAMGS0,    PAGE = 1
   ramgs1           : > RAMGS1,    PAGE = 1
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   dclfuncs         : > FLASH_BANK0_SEC1,     PAGE = 0, ALIGN(4)


#if defined(__TI_EABI__)
    /* CLA specific sections */
    Cla1Prog        : LOAD = FLASH_BANK0_SEC4,
                      RUN = RAMLS0,
                      LOAD_START(Cla1ProgLoadStart),
                      RUN_START(Cla1ProgRunStart),
                      LOAD_SIZE(Cla1ProgLoadSize),
                      PAGE = 0, ALIGN(4)
#else
    /* CLA specific sections */
    Cla1Prog        : LOAD = FLASH_BANK0_SEC4,
                      RUN = RAMLS0,
                      LOAD_START(_Cla1ProgLoadStart),
                      RUN_START(_Cla1ProgRunStart),
                      LOAD_SIZE(_Cla1ProgLoadSize),
                      PAGE = 0, ALIGN(4)
#endif
 
    
    Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW,   PAGE = 1
    CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH,  PAGE = 1

#if defined(__TI_EABI__)
   .TI.ramfunc      : LOAD = FLASH_BANK0_SEC1,
                      RUN = RAMLS4
                      LOAD_START(RamfuncsLoadStart),
                      LOAD_SIZE(RamfuncsLoadSize),
                      LOAD_END(RamfuncsLoadEnd),
                      RUN_START(RamfuncsRunStart),
                      RUN_SIZE(RamfuncsRunSize),
                      RUN_END(RamfuncsRunEnd),
                      PAGE = 0, ALIGN(4)
#else
   .TI.ramfunc      : LOAD = FLASH_BANK0_SEC1,
                      RUN = RAMLS4
                      LOAD_START(_RamfuncsLoadStart),
                      LOAD_SIZE(_RamfuncsLoadSize),
                      LOAD_END(_RamfuncsLoadEnd),
                      RUN_START(_RamfuncsRunStart),
                      RUN_SIZE(_RamfuncsRunSize),
                      RUN_END(_RamfuncsRunEnd),
                      PAGE = 0, ALIGN(4)
#endif

   .scratchpad      : > RAMLS1,           PAGE = 1
   .bss_cla         : > RAMLS1,           PAGE = 1

   Cla1DataRam      : > RAMLS2,           PAGE = 1
   cla_shared       : > RAMLS1,           PAGE = 1
   CLADataLS1       : > RAMLS1,           PAGE = 1

#if defined(__TI_EABI__)
   .const_cla      : LOAD = FLASH_BANK0_SEC2,
                      RUN = RAMLS3,
                      RUN_START(Cla1ConstRunStart),
                      LOAD_START(Cla1ConstLoadStart),
                      LOAD_SIZE(Cla1ConstLoadSize),
                      PAGE = 0, ALIGN(4)
#else
   .const_cla      : LOAD = FLASH_BANK0_SEC2,
                      RUN = RAMLS3,
                      RUN_START(_Cla1ConstRunStart),
                      LOAD_START(_Cla1ConstLoadStart),
                      LOAD_SIZE(_Cla1ConstLoadSize),
                      PAGE = 0, ALIGN(4)
#endif
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/