Part Number: TMS320F2800152-Q1
Other Parts Discussed in Thread: C2000WARE
Dear champs,
I ask this for our customer.
Q1. Is the physical distribution of C2000's Flash as shown in the figure below?

If Q1 is correct,
Q2. The Flash of the C2000 series does not support byte access and can only access (Read/Write) one Word at a time? So, Flash cannot be accessed at odd addresses?
Q3. In the Linker file, the length of the section I defined actually occupies twice the space as defined?
As shown in the figure below, the linker file, HEADERINFO, has a length of 0x100. Is this in word units? That is to say, "The length of the HEADERINFO segment is 0x100 Word, that is, 256 words, 512 Byte?"

Thanks!
Best Regards,
Julia