Part Number: TMS320F28377D
Hi E2E,
I have an inverter using a TMS320F28377D, configured to use the digital comparators for phase over-current detection as well as DC bus over-voltage. Running at a light load on this inverter and everything behaves fine. Additionally, previous designs using the same circuitry and configuration, everything behaves fine. Once I get to a certain operating point, at relatively "high" voltage for our application, I start to see all four of these comparators trip at the same time. I should note I'm running at about one third of my expected trip point for current and at about two thirds of the trip point for voltage.
I've done a few different things for debug so far. The first is turning off the trip zone functionality and datalogging how many times I get the digital comparators tripping, by immediately clearing them if they trip. The comparators trip proportional to my load, which sort of would indicate noise to me.
Is there some mechanism or means in the digital comparator block or the Xbar block that might cause these to all trip at the same time under some condition?
Regards,
Noah E