Other Parts Discussed in Thread: C2000WARE
I am new to this dual core controller
I have added CPU1 in predefined symbol.
And started a test code.


"C:\\ti\\ccs1240\\ccs\\utils\\bin\\gmake" -k -j 8 all -O
Building target: "test.out"
Invoking: C2000 Linker
"C:/ti/ccs1240/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcrc --fp_mode=relaxed --advice:performance=all --define=CPU1 -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi -z -m"test.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccs1240/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib" -i"C:/ti/ccs1240/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="test_linkInfo.xml" --rom_model -o "test.out" "./f28p65x_codestartbranch.obj" "./f28p65x_cputimers.obj" "./f28p65x_dbgier.obj" "./f28p65x_defaultisr.obj" "./f28p65x_dma.obj" "./f28p65x_gpio.obj" "./f28p65x_piectrl.obj" "./f28p65x_pievect.obj" "./f28p65x_sdfm_drivers.obj" "./f28p65x_struct.obj" "./f28p65x_sysctrl.obj" "./f28p65x_tempsensorconv.obj" "./f28p65x_usdelay.obj" "./main.obj" "../28p65x_generic_ram_lnk_cpu1.cmd" -llibc.a
<Linking>
undefined first referenced
symbol in file
--------- ----------------
ClkCfgRegs ./f28p65x_sysctrl.obj
CpuSysRegs ./f28p65x_sysctrl.obj
Dcc0Regs ./f28p65x_sysctrl.obj
Dcc1Regs ./f28p65x_sysctrl.obj
WdRegs ./f28p65x_sysctrl.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "test.out" not built
>> Compilation failure
makefile:148: recipe for target 'test.out' failed
gmake[1]: *** [test.out] Error 1
makefile:144: recipe for target 'all' failed
gmake: *** [all] Error 2
If any one have idea please let me know.