Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG, , C2000WARE
I am currently learning to write code for TMS320F280039C. I using sysconfig to setup the I2C registers. After loading the code, I checked the SCL line and its showing 0.043v. I wrote a program that would write some data to MCP4725. Just before data is transferred to the registers, I check whether the bus is busy or not by calling the function I2C_isBusBusy(). Every time when I try to transmit, the I2C_isBusBusy returns true.

I am using MCP4725 module as a slave device and it has a 4.7k pull resistors on both SCL and SDA.
main.c
#include "board.h"
#include "device.h"
#include "driverlib.h"
#include "src/App/uart.h"
#include "src/Drivers/i2c.h"
#include <stdio.h>
//
// Main
__interrupt void INT_myI2C0_ISR(void);
__interrupt void INT_myI2C0_FIFO_ISR(void);
uint16_t trxBuff[3] = {0x1, 0x2, 0x3};
char data[100] = "Hello world";
I2C_Data_s I2C_Params = {.Data = trxBuff, .Data_Length = 3, .Peripherial_Address = 0x60};
void main(void) {
// Device Initialization
Device_init();
//
// Initializes Peripheral Interrupt Expansion module (PIE) and clears PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initializes the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
Board_init();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
sprintf(data, "Programmed stated");
while (1) {
I2C_Transmit(myI2C0_BASE, &I2C_Params);
while (I2C_Params.Status == PENDING)
;
GPIO_togglePin(myGPIO0 );
DEVICE_DELAY_US(250000);
GPIO_togglePin(myGPIO0 );
DEVICE_DELAY_US(250000);
}
}
__interrupt void INT_myI2C0_ISR() {
handleI2C_Interrupts(myI2C0_BASE,&I2C_Params);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
};
__interrupt void INT_myI2C0_FIFO_ISR() {
sprintf(data, "FIFO Interrupt");
UART_TX(data);
};
i2c.c
#include "i2c.h"
#include "board.h"
#include "driverlib.h"
static uint8_t totalDataSend = 0;
void I2C_Initialize() {
}
I2C_Status_TypDef checkBusStatus(uint32_t base) {
if (I2C_isBusBusy(base)) {
return ERROR_BUS_BUSY;
}
if (I2C_getStopConditionStatus(base)) {
return ERROR_STOP_NOT_READY;
}
return SUCCESS;
}
void I2C_Transmit(uint32_t base, I2C_Data_s *I2C_Params) {
ASSERT(I2C_isBaseValid(base));
I2C_Status_TypDef status;
status = checkBusStatus(base);
if (status != SUCCESS) {
I2C_Params->Status = status;
} else {
I2C_disableModule(myI2C0_BASE);
I2C_setConfig(base, (I2C_CONTROLLER_SEND_MODE));
I2C_setTargetAddress(base, I2C_Params->Peripherial_Address);
I2C_setDataCount(base, I2C_Params->Data_Length);
I2C_enableModule(myI2C0_BASE);
// for (int i = 0; i < I2C_Params->Data_Length; i++)
// {
// I2C_putData(base, *(I2C_Params->Data + i));
// }
I2C_Params->Status = PENDING;
I2C_sendStartCondition(base);
}
}
void I2C_Recieve(uint32_t base, I2C_Data_s *I2C_Params) {
ASSERT(I2C_isBaseValid(base));
I2C_setConfig(base, (I2C_CONTROLLER_RECEIVE_MODE));
I2C_setTargetAddress(base, I2C_Params->Peripherial_Address);
I2C_setDataCount(base, I2C_Params->Data_Length);
// for (int i = 0; i < I2C_Params->Data_Length; i++)
// {
// I2C_putData(base, *(I2C_Params->Data + i));
// }
I2C_Params->Status = PENDING;
I2C_sendStartCondition(base);
}
void handleI2C_Interrupts(uint32_t base, I2C_Data_s *I2C_Params) {
I2C_InterruptSource intSource = I2C_getInterruptSource(base);
if (I2C_getStatus(base) & I2C_STS_NO_ACK) {
I2C_clearStatus(base, I2C_STS_NO_ACK);
I2C_sendStopCondition(base);
}
switch (intSource) {
case I2C_INTSRC_ARB_LOST:
// Report Arbitration lost failure
I2C_Params->Status = ERROR_ARBITRATION_LOST;
break;
case I2C_INTSRC_NO_ACK:
// Clear NACK flag and generate STOP condition on a NACK condition
I2C_clearStatus(base, I2C_STS_NO_ACK);
I2C_sendStopCondition(base);
I2C_Params->Status = ERROR_NACK_RECEIVED;
break;
case I2C_INTSRC_REG_ACCESS_RDY:
I2C_clearStatus(base, I2C_STS_RX_DATA_RDY);
break;
case I2C_INTSRC_RX_DATA_RDY: {
if (totalDataSend < I2C_Params->Data_Length)
*(I2C_Params->Data + totalDataSend) = I2C_getData(base);
else {
I2C_sendNACK(base);
I2C_sendStopCondition(base);
}
totalDataSend = totalDataSend + 1;
break;
}
case I2C_INTSRC_TX_DATA_RDY:
if (totalDataSend < I2C_Params->Data_Length) {
I2C_putData(base, *(I2C_Params->Data + totalDataSend));
I2C_sendStopCondition(base);
} else {
I2C_Params->Status = SUCCESS;
}
totalDataSend = totalDataSend + 1;
break;
case I2C_INTSRC_STOP_CONDITION:
// I2C_disableInterrupt(base, (I2C_INT_TXFF | I2C_INT_RXFF));
// I2C_Params->pTX_MsgBuffer = TX_MsgBuffer;
// I2C_Params->pRX_MsgBuffer = RX_MsgBuffer;
// I2C_disableFIFO(base);
break;
case I2C_INTSRC_ADDR_TARGET:
break;
}
}