This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to use GPIO6/XINT1 to capture/measure a PWM signal. (ECAP pins are not available)
I am seeing a mismatch between the measurements and what I am expecting based on the TRM and the input at the pin
As a test, I am generating a 10khz PWM signal with 50% duty from EPWM3, and have this connected to GPIO6.
Pulse high time = pulse low time = 50us
Pulse period = 100us
From the TRM, xintctr clock source is SYSCLKOUT
SYSCLK = 60MHz
So my expectation is that the 50us hightime or lowtime would be 3000 counts of a 60MHz clock. Instead I'm seeing a measurement of 50 for hightime and ~227 for lowtime.
At initialization, I first set POLARITY to rising edge only, so I know which edge is being captured. At first capture, I switch POLARITY to both edges. Below is the code used for init and ISR:
Initialization:
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; // 0=GPIO, 1=EPWM1A, 2=Resv, 3=Resv
GpioCtrlRegs.GPADIR.bit.GPIO6 = 0; // 1=OUTput, 0=INput
GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL = 6; // GPIO6 as interrupt source
XIntruptRegs.XINT1CR.bit.POLARITY = 0x1; // Trigger on rising edge to start
xint1_startup_flag = true;
XIntruptRegs.XINT1CR.bit.ENABLE = 0x1;
EDIS;
ISR:
if (xint1_startup_flag){
xint1_startup_flag = false;
XIntruptRegs.XINT1CR.bit.POLARITY = 0x3;
xint1_nextedge_is_falling=true;
}
else{
if(xint1_nextedge_is_falling){
xint1_nextedge_is_falling=false;
xint1_pulse_high_time = XIntruptRegs.XINT1CTR; // READING 50, EXPECTING 3000
}
else{
xint1_nextedge_is_falling=true;
xint1_pulse_low_time = XIntruptRegs.XINT1CTR; // READING ~220, EXPECTING 3000
}
}
I confirmed via logic analyzer that the PWM waveform is correct: 50% duty at 10kHz. Test hardware is the LaunchPadXL for the 28027.
Do you have suggestions why I'm getting these measurements instead of the expected values? Or is my interpretation of the datasheet mistaken?
Thanks!
I've reduced the input PWM frequency to 5khz, still at 50% duty, and the values that I'm ready from XINTCTR do not change much.
Thanks,
So, regardless of your PWM frequency, XINTCTR value doesn't change much? I presume you have verified that SYSCLKOUT is 60MHZ. Can you please send me your code? You can share it with me privately, if you want. You can do this by initiating a friendship request with me first. You can do so by choosing the "Request Friendship" option when you hover the cursor over my name
The EPWM3 timing is working as expected to generate the PWM, so that is my indication that SYSCLKOUT is operating at 60MHz. (In addition to confirming the setting in DeviceInit)
Understand. Do you see the incorrect value in the register as well? i.e. instead of reading the value through a variable, look at the value of XINTCTR in the register window.
XINTCTR does not freeze when I reach the XINT ISR. However, when the EPWM is running, I see that the value of XINTCTR in the register window is showing values greater that 50 or 270, possibly up to 3000. So maybe it is a matter of not reading the register correctly?
I am using
uint16_t xint1_pulse_high_time;
xint1_pulse_high_time = XIntruptRegs.XINT1CTR;
XIntruptRegs is from TI libraries...I'll look into this to see if it mapped correctly.
So maybe it is a matter of not reading the register correctly?
I also feel the register is not being read properly.
Few ideas to try:
Mark,
One more idea to try: Do not involve the PWM at all. Just toggle a GPIO pin (as a GPIO) and measure the pulse width. This can be achieved just a few lines of code
Hi Hareesh,
After re-reading the description of XINTCTR, maybe this is an issue of making a wrong assumption about how to use XINTCTR. From the TRM section 1.6.5.2, the counter is reset to 0 on an interrupt edge. So this is the reason that I'm reading values near-zero in the ISR. The ISR is triggered, but XINTCTR has just been cleared.
Which leads to a follow-on question...what is the use case of XINTCTR? Section 1.6.5.2 also says "These counters can be used to accurately time stamp an occurrence of the interrupt". How does this work if XINTCTR is zero at the interrupt? It seems like there should be a capture register for this to work.
Thanks for your help.
the counter is reset to 0 on an interrupt edge.
Mark, I missed that subtlety. Thanks for pointing that out. It's been ages since I worked on this peripheral.
what is the use case of XINTCTR?
If the count is read, it tells you how long ago the edge was detected.
It seems like there should be a capture register for this to work.
For what you were attempting to do, you need to use the Capture unit.