Part Number: LAUNCHXL-F2800137
We are exploring option to flash code through XDS110 Debug Probe. But getting error while test connection.
Error:
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-267' (0xfffffef5).
The title is 'SC_ERR_XDS110_TARGET_SUPPLY'.
The explanation is:
The controller could not detect valid target supply. Check target
JTAG connection and/or connection setting specifying voltage level.
[End: Texas Instruments XDS110 USB Debug Probe_0].
Following is Pin mapping for the reference:
|
XDS110 Debug Probe
|
LaunchXL-F2800137
|
|
Expansion Header - pin 25
|
J1/J3 GND
|
|
Expansion Header - pin 27
|
3v3
|
|
Debug 20 to 14 pin extension - pin 1
|
TMS
|
|
Debug 20 to 14 pin extension - pin 11
|
TCK
|
|
Debug 20 to 14 pin extension - pin 7
|
TDO
|
|
Debug 20 to 14 pin extension - pin 3
|
TDI
|
we have also check with below mapping, but getting same error.
| XDS110 Debug Probe | LaunchXL-F2800137 |
| Debug 20 to 14 pin extension - pin 8 | J1/J3 GND |
| Debug 20 to 14 pin extension - pin 5 | 3v3 |
| Debug 20 to 14 pin extension - pin 1 | TMS |
| Debug 20 to 14 pin extension - pin 11 | TCK |
| Debug 20 to 14 pin extension - pin 7 | TDO |
| Debug 20 to 14 pin extension - pin 3 | TDI |