This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have transitioned from using the F28379D microcontroller to the F28388D microcontroller in our design. I would like to inquire if our existing Design Drive Development Kit, which we previously used, is still compatible with the new evaluation board for the F28388D microcontroller.
If it is possible, could you also please advise if there is anything I need to consider when using the Development Kit with the new evaluation board?
Thank you for your assistance.
Best regards,
Wilko
Hi Wilko,
Yes - TMDXIDDK379D kit is compatible with TMDSCNCD28388D control card as well. You can also refer the examples for the same in the latest MotorControlSDK "...\ti\c2000\C2000Ware_MotorControl_SDK_5_01_00_00\solutions\tmdxiddk379d\f2838x"
Sumit