This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28378S: After enabling DCSM no access to flash bank 1

Expert 2730 points

Part Number: TMS320F28378S
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

After enabling the DCSM to dedicate all RAM and Flash to Z1, I can't access Flash bank 1. Here is the configuration I used:

.sect "dcsm_zsel_z1"
      .retain
      .long 0x000000FF       ;Z1-EXEONLYRAM
      .long 0x00003FFF      ;Z1-EXEONLYSECT
      .long 0x10005555          ;Z1-GRABRAM
      .long 0x15555555         ;Z1-GRABSECT

The whole bank 1 should be under Z1 or not? I can't read (for example 0x0C0000) from debugger or direct from code. Am I missing something? Without DCSM everything works as it should.

In dcsm_security_tool example, it is not possible to configure flash bank 1 at all! If one uses the example then the flash bank 1 access will be set to 0 = Invalid. Flash BANK1 is inaccessible.