Champs:
#1.
My customer has surveyed this E2E
#2.
Now, his questions are:
Currently, in my application, some of the CMPSS CTRIPs are routed through EPWM XBAR and configured as either CBC mode or OST.
I'd like to inquire:
- Whether using OST mode would mitigate the ADC accuracy issue? thereby allowing the simultaneous usage of ADC and CMPSS on the same pin?
2..Conversely, CBC mode is not recommended?
3..Is there any evidence or some reports regarding the accuracy issue when simultaneously using CMPSS and ADC?
Please comment, thanks.
BR Rio