This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: Is it possible to use an internal regulator ?

Genius 3215 points

Part Number: TMS320F28384D

Hi All,

Is it possible to use an internal regulator with the TMS320F28384D?
Can it be started with a single 3.3V power supply?

Best Regsrds, 

Ito

  • Ito,

    This device does not have an internal voltage regulator on it, so it is not possible.  There is a NC pin for compatibility reasons with the F2837x device, but this pin does not route to any logic on the device.

    Best,

    Matthew